This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于变压器的输入为方波的问题



        我想要通过变压器耦合电感的方式来实现方波信号幅值的放大,在一篇文章中看到了附件中的原理框图(图1),在multisim中用一个简单的电路进行仿真模拟(图2),图中XFG2输出为频率为1MHZ,高电平为+5V,低电平为0V的方波信号,输入到NMOS管作为开关,可是实际仿真中MOS管的VDS的电压如图3所示,可以看到有很大的电压尖峰,后来查找资料,发现和DC-DC中的隔离flyback电路很相似,然后将仿真电路改为如图4所示,可是VDS的电压显示如图5所示,并没有多少改善,我想请教一下,这种方法能否实现方波信号幅值的放大,时候是我参数选择的不对造成的这种结果?

方波.doc
  • 你好,不是很清楚你是需要对一个方波信号进行放大,还是想设计反激变换器。如果只是想放大方波信号,变压器可以完成,但变压器只能变换纯交流电压信号。所以你的方波如果存在直流偏置,可以在输入端串个电容。

    另外,反激变压器其实严格来说更像个电感,用来做你说的信号放大不合适。1MHz的开关频率是比较高的了,你的波形应该是结电容的充放电现象。

  • 你好,我需要的是对方波信号的幅值进行放大,将高电平为+3.3V,低电平为0V的方波,通过变压器变为高电平为+15V,低电平为0V的方波信号,我根据你所说的串入了一个隔直电容,可是,效果并不理想,能否给出具体点的原理图或者电路图,我对于变压器的了解比较少,谢谢!