我想要通过变压器耦合电感的方式来实现方波信号幅值的放大,在一篇文章中看到了附件中的原理框图(图1),在multisim中用一个简单的电路进行仿真模拟(图2),图中XFG2输出为频率为1MHZ,高电平为+5V,低电平为0V的方波信号,输入到NMOS管作为开关,可是实际仿真中MOS管的VDS的电压如图3所示,可以看到有很大的电压尖峰,后来查找资料,发现和DC-DC中的隔离flyback电路很相似,然后将仿真电路改为如图4所示,可是VDS的电压显示如图5所示,并没有多少改善,我想请教一下,这种方法能否实现方波信号幅值的放大,时候是我参数选择的不对造成的这种结果?