This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713: 单节电池应用方案供电咨询

Part Number: BQ25713


芯片采用BQ25713:

1)VBUS输入采用电源适配器5V 3A输入;

2)电池为单节磷酸铁锂电池3并(1S3P),电压范围2.8V~3.6V;

3)VSYS输出电压为5V 6A;

叫教下如果我去掉上述红框内3V3,仅电池供电,VSYS是否可以输出5V;

如果不能还行需要确保哪些电路的设计。