Part Number: LP2992
输入:5.5V,输出:3.3V,负载:100ma
发生VOUT和VIN短路的问题,输出只有1.6V,芯片发烫严重
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
一般LDO损坏都是过压,因为过载都会保护。
但是从你描述看5.5V输入距离16V的输入上限很远,不应该是过压。
请问你是哪种封装?SOT23,还是WSON? 不良率多少?