hi Sir,
目前有一案件使用BQ40Z50-R1 / 1S1P / 4040mAh, 按造正常learning程序去進行是正常的 ( CHEM ID:2052 , 使用範圍電壓 : 4.2V ~ 3.0V ) updata = 06
後因客戶系統設計調整 Term V = 3000mV to 3450mV, 則無法更新Qmax , 且發現 RSOC 在充電中3.7V以下是不會計算的
現在已重新調整參數進行learning則依樣Qmax不會更新過去
GG 如附件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi Sir,
目前有一案件使用BQ40Z50-R1 / 1S1P / 4040mAh, 按造正常learning程序去進行是正常的 ( CHEM ID:2052 , 使用範圍電壓 : 4.2V ~ 3.0V ) updata = 06
後因客戶系統設計調整 Term V = 3000mV to 3450mV, 則無法更新Qmax , 且發現 RSOC 在充電中3.7V以下是不會計算的
現在已重新調整參數進行learning則依樣Qmax不會更新過去
GG 如附件
您好,请参考文档的2.3.5 电量计 Golden Learning 易错分析www.ti.com.cn/.../zhcaaf7
hi Star,
目前使用方式有按造2.3.5要求進行
電池容量4040mAh 改設定Design Capacity mAh = 2880, Design Capacity cWh = 1036cWh
(以上設定為預估客戶的使用容量變成4.2V ~ 3.45V )
充電4.2V/1A/cut off 120mA
放電使用0.28C (0.808A) to 3450mV
仍無法更新Qmax / FCC / 另RSOC 在充放電中3.7V以上才開始進行計算以下為本次的log data2022-12-28_3450.xlsx
您好,已经在E2E英文论坛发帖询问更了解这款芯片的TI工程师,请继续关注。
e2e.ti.com/.../bq40z50-r1-bq40z50-r1-change-the-term-v-from-3000mv-to-3450mv-qmax-update-fail
您好
Setting TermV to high voltages like 3400 mV can cause gauging issues since voltage might fall in the flat zone and it is hard for the gauge to predict. Also, if TermV is set to 3400 mV and a big load is present, the loaded cell voltage could fall near EDV even with a charged cell of 3700 mV. At this point SOC will drop to 0%.
For this it is recommended to increase Reserve Capacity and lower/keep TermV near 3000mV. This is a trial error test, and customer will need to do it several times until gauge is best tuned.
I suggest following section 3 from the below app note. SLUA948
https://www.ti.com/lit/an/slua948/slua948.pdf?ts=1672327212389&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FBQ27426%253Futm_source%253Dgoogle%2526utm_medium%253Dcpc%2526utm_campaign%253Dapp-null-null-GPN_EN-cpc-pf-google-wwe%2526utm_content%253DBQ27426%2526ds_k%253DBQ27426%2526DCM%253Dyes%2526%2526utm_source%253Dgoogle%2526utm_medium%253Dcpc%2526utm_campaign%253D%2526utm_content%253D%2526ds_k%253Dbq27426%2526DCM%253Dyes%2526gclid%253DCjwKCAiAkrWdBhBkEiwAZ9cdcOudzbU-KFBkP8w5-wbuQRoGfs47MMaM2Xxq0dmVIOSkPWtUyykPmBoCnGsQAvD_BwE%2526gclsrc%253Daw.ds
hi Star,
1. 2023-01-03 modify design cap 3950mAh to 2880mAh / Term V 3000mV to 3450mV / Reserve Cap-mAh 1550mAh
2. 2023-01-04 modify design cap 3950mAh to 2880mAh / Term V 3000mV to 3450mV
在1狀況下 充電RSOC /RC很久時間以後才會開始計數 + QMAX 不更新,
在2狀況下 充電RSOC /RC會正常計數 BUT QMAX 不更新,
請問是否用2的狀況使用是沒有問題的
hi Star,
應該說目前多顆測試是正常的的RSOC跳動,FCC/RM/RA table 等都有更新且符合之前正常充放的曲線,但唯獨Qmax 沒有更新這點我不能確認是否GG後續計算是否正常
另案多種測試條件下,使用Reserve Cap-mAh這個方式是不太能正常計算RSOC/FCC/RM ( 這邊均在3.7V以上才會開始計算跳動)
只能將原額定容量(Design capacity)下修的方式去進行learning才可以正確地計算RSOC
您好,
There is a misunderstanding, please let me be more clear.
您好,E2E英文论坛的工程师已经在跟进,请继续关注。
e2e.ti.com/.../bq40z50-r1-bq40z50-r1-change-the-term-v-from-3000mv-to-3450mv-qmax-update-fail