This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: 多次切換會latch輸出

Part Number: TPS2121

hi sir,

請問下使用EVM進行驗證,目前設計使用方式中有遇到latch問題 (LIN 設定 4.5A / PRI = 12V / CP2 = NA / ST=GND / )

1. 使用power supply *2 input → IN1:6.6V ,  IN2:6.2V , E-LOAD : 2.5A ( or 16W )

2. 確認 IN1 持續附載 2.5A

3. IN1 6.6V SW to 4.0V ( E-load keep 2.5A ) change to IN2 - ( PASS )

4. IN1 4.0V SW to 6.6V ( E-load keep 2.5A ) 此時輸出 latch 電壓 =0V

想確認:

1. 以上動作是否正確

2. 是否有設定可以調整 IN1 輸出多次切換而不會LACTCH