This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63700: 错误输出正电压

Part Number: TPS63700


5V电压转成-5V电压

原理图参考技术手册,相同

但是各个引脚输出电压都和手册上不一样

1脚:2.65V

6脚:5V

8脚:2.76V

9脚:1.5V

技术手册上

8脚:-5V

9脚:0V

请求各位大佬伸出援手,谢谢