This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: TL431Vref及Vo电压波动较大

Part Number: TL431


你好!

我们现在正使用TL431设计一个输出为6V的基准电压电路以供AD采样使用,电路图如下

调试过程中,我们更改了R4和R7的位置(以实现Vo=(1+R4/R7)*2.5=6.06V),拆除了C9和R3,同时也按照手册说明尝试更改C4电容值,效果一般,因此最后选择拆除C4。

现在的问题是:使用万用表测试TL431的Ref引脚为2.5V,但是使用示波器观测发现,该电压存在较大波动,可达60mV甚至100mV,同时,6V输出电压波动可达100mV。

TL431的Ref电压波形图如下

请问,产生该问题的可能的原因有哪些?我们接下来该如何改进电路?

非常感谢!