以上是LM5010SD的应用,输入40-60V 输出15V 0.8A ,工作不到10分钟就过温保护了,芯片温度高达150C
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Michael Yang 谢谢你给的宝贵意见,我现在的LM5010SD底部没有接到铜箔上散热,如果接上去温度会不会降很多?
这个是电流仿真型的buck电路,开关管集成在内部,所以外部的散热措施尤为重要,
芯片底部的thermal pad是内部die散热的重要路径,此外还可以起到屏蔽die的作用,将其与接地的铜箔焊接好。
Hi
如上所谈,PowerPAD接GND的重要性,事实上芯片是将GND铜箔当做散热片散热,所以不仅要焊接还要充分焊接,GND的面积也要尽量扩展,包括打孔到背面,连接更大面积的GND.
可以参考其EVM layout: http://www.ti.com.cn/cn/lit/ug/snva101a/snva101a.pdf
谢谢,热问题得以解决,但目前试产100PCS发现LM5010SD有18PCS无输出,经分析发现2脚BST与9脚VCC之间击穿。经测试50V输入时2脚与9脚的峰值70V未超过规格书里的76V,准备进入量产,不良率太高,有点头疼。