LM5071采用非隔离方式输出,只知道调节R12的阻值可以改变输出电压,但是不知道具体是怎么计算出来的,如果想输出其他电压该如何选择电阻值。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
按照这个电路,因为2个三极管的极电压相同,也就是发射极电压也一样,即R11加上R12两个电阻上的压降是等于输出电压的,可依据如下公式:
FB= Vo/ (R11+R12) * R18=1.25mV(tipcal) ----- R11+R12上的电流等于R18上的电流, 所以修改这三个电路都可以影响输出电压,但是R11其实可以不要的。
Hi
另外需要指出的是,不同的输出电压,对于电感的选择,以及补偿电路都是有影响的,所以您还可能需要修改这些参数以达到最佳性能。