This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27525: Pspice model unencrypted version

Part Number: UCC27525


I would like to use UCC27525 PSpice model, but it does not work. And my simetrix version is full version, so I can successfully imported the gate driver. But I can not run the circuit because of the gate driver. There are a lot of errors:

UCC27525_TRANS.lib (71): ...

*** ERROR *** Missing nodes. This device has 2 terminals

UCC27525_TRANS.lib (73): ...

*** ERROR *** No model name specified

UCC27525_TRANS.lib (75): ...

*** ERROR *** Missing nodes

UCC27525_TRANS.lib (77): ...

*** ERROR *** Missing nodes. This device has 2 terminals

UCC27525_TRANS.lib (80): ...

*** ERROR *** Missing nodes

UCC27525_TRANS.lib (82): ...

*** ERROR *** Missing nodes. This device has 2 terminals

And I want have a really usable UCC27525 Unencrypted PSpice Transient Model.