Part Number: UCC27525
I would like to use UCC27525 PSpice model, but it does not work. And my simetrix version is full version, so I can successfully imported the gate driver. But I can not run the circuit because of the gate driver. There are a lot of errors:
UCC27525_TRANS.lib (71): ...
*** ERROR *** Missing nodes. This device has 2 terminals
UCC27525_TRANS.lib (73): ...
*** ERROR *** No model name specified
UCC27525_TRANS.lib (75): ...
*** ERROR *** Missing nodes
UCC27525_TRANS.lib (77): ...
*** ERROR *** Missing nodes. This device has 2 terminals
UCC27525_TRANS.lib (80): ...
*** ERROR *** Missing nodes
UCC27525_TRANS.lib (82): ...
*** ERROR *** Missing nodes. This device has 2 terminals
And I want have a really usable UCC27525 Unencrypted PSpice Transient Model.