This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在使用lmr62014时,希望输入11v~12v,输出12v,最大电流1a,实际中电压波动很大,想问一下可能是什么问题,电感用的22uh,按数据手册上所标示,R1=100K,R2=11K,C2=10UF/25V
Hi
请提供完整的电路图。 其中推荐输入输出选择低ESR的陶瓷电容,另外测试时采用0.5~0.8A的负载,看是否输出能稳定下来?
感谢您的回复,这个问题目前已经解决,不是我设计的原因,是其中一个分压电阻坏了,连续测试了8个小时,工作比较稳定,目前还在考机