Other Parts Discussed in Thread: TPS5430, TPS54331
RT,规格书只提到了输入7V-28V可以输出3.3V@3A,那么输入5V是否也可以,芯片还没买到,先来问问,谢谢!
另外TPS5430是否有PIN2PIN的,支持5V输入的芯片呢?
用于USB供电的设备,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是否可以理解为当boot电容两端电压低于2.1V时,输出电压将降低到内部基准电压?
空载的话有具体限定吗?10mA的负载算不算空载?谢谢!
不是降到基准电压,是上管无法开通,输出掉落到一定值使boot电压可以高于2.1V时才会开关动作使输出上升。
一般情况下空载下会出现如上情况,加10mA左右的假负载就可以解决空载掉落的问题,具体可以再电路上作测试。
当然,如果输入输出电压差够大,不存在这个问题。
这个与输入输出压差有关系,当输出输入压差较小并且空载时,占空比很大,即下管导通的时间很短,所以boot电容在下管导通时并未充到2.1V,所以下个开关周期上管不会导通,在这种情况下,输出电压自动会降低,从而减小占空比,增加下管导通时间,使boot电容有效充电。
Hi
补充一下,随着输入电压的降低,占空比曾高,流过MOS的电流增大,芯片的温度是越高的。
按照TI webench仿真, 5V转3.3V/2.3A时,芯片的温度已经高达121℃(环境温度30℃,热阻100℃/W), 所以你应用如果需要较低的输入电压,并且希望得到3A的最大负载电流,需要选择带PowerPad封装的,或者额外的散热设计。
这个估计不能接受,能推荐一颗5V输入,3.3V&2A输出的DCDC吗?
需要容易购买的,单价8rmb一下的,谢谢!