This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331在输入5V时是否可以输出3.3V@3A?

Other Parts Discussed in Thread: TPS5430, TPS54331

RT,规格书只提到了输入7V-28V可以输出3.3V@3A,那么输入5V是否也可以,芯片还没买到,先来问问,谢谢!

另外TPS5430是否有PIN2PIN的,支持5V输入的芯片呢?

用于USB供电的设备,谢谢!