如题:
输出电压:31.2V,电流:0.98A; 输入电压:36V;
接10串3并COB灯珠;
在环境温度32度左右;LM3414HV表面温度86度,
在环境温度50度下;LM3414HV表面温度90度;
请问有什么方法整改;附件为PCB文件;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请参考附件资料。
在250KHZ的情况下,LM3414HV评估板上在测得LM3414HV在常温30度下,其结温81度。
在575KHZ的情况下,LM3414HV评估板上在测得LM3414HV在常温30度下,其结温101度。
以此,可以通过减低工作频率和扩大PCB散热面积来降低IC的温度。需要注意的是,降低频率会增大输出纹波,但可以通过加大电感值和输出电容来优化。
如果板的体积受到严格限制,以上措施改善LM3414HV的温度不大的情况下,建议采用LM3409HV的芯片,通过外部MOS的方式,可以大大提供效率,降低IC的温升,但是成本也就相应地增加了。