This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的输入电压为24~100V,想通过此BOOST电路得到120V输出电压。控制芯片用UC2843,其中J1端为可调变压器输入端,J2端接负载电阻。UC2843的工作电源VCC我用线性电压源来提供,所有的地都接在一块的。现在的情况是,当UC2843的VCC没有电压时,MOS管正常关断,可是,当把VCC接上时,MOS管发热严重,并且输入端J1电压降到很低(没有接VCC时,J1端电压为40V,接上VCC后,J1端电压降为2.5V左右)。我感觉是,接上VCC后,MOS管就导通了,但是一直不能关断,导致输入有短路现象。请问这个是什么原因呢?
HI
首先你要确认一下你的电路,是否有输入电容(在电路图上没有?)
其次确认一下负载多大,电感的饱和电流是否足够?
你好,我的输入端是有电容的,整流滤波的电容;请问这个有影响吗?输出端接的是400ohm的大功率水泥电阻,我认为就电感的线径来说,电感电流不会饱和。但是会出现嗤嗤的声音。请问这是什么原因呢?
你好,我的输入端是有电容的,整流滤波的电容;请问这个有影响吗?输出端接的是400ohm的大功率水泥电阻,我认为就电感的线径来说,电感电流不会饱和。但是会出现嗤嗤的声音。请问这是什么原因呢?