您好:
我用BQ24600 IC充3串(12.6V)锂电池时,IC很发热。原理图是按照TI管网上提供的。测试R6(10R)电阻处电流,115mA应该是正常的。请问是什么原因照成?要怎么改善?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
,好像电源指示不正常。好像STAT和\PG都是低电平。你贴的是ti的原理图,给予的信息比较有限。STAT/ \PG为低应该是正常工作状态。请仔细对比原理图和所贴物料是否对应。查看以下各条件是否满足:
• CE is HIGH
• The device is not in VCCLOWV mode
• The device is not in SLEEP mode
• The VCC voltage is lower than the ac overvoltage threshold (VCC < V ACOV )
• 30-ms delay is complete after initial power up
• The REGN LDO and VREF LDO voltages are at the correct levels
• Thermal shut (TSHUT) is not valid
• TS fault is not detected
在上电的时候抓取VCC, /PG, VREF, REGN的波形,看是否有异常。查看 PH, LODRV, CE 波形看是否有异常
你好:
你上面提到的条件都满足的,只是我用的mosfet是IRF7831.不知道有没有影响。我把layout的原理图发给你分析一下。
Thanks!
nathanxiang
原理图是正确的,你是需要3A 快速充电电流吧?MOSFET应该影响不大。你现在的问题只是芯片的耗电太大,芯片太热了了吗?其它功能是否正常工作,有没有用示波器测试Vout, 充电电流,Vbat, TS, 及PH的波形,看和EVM板对比一下,波形是否有异常。另外,附上layout培训资料。
正常充电时的典型工作电流为50mA.加大电阻没有多大作用。如果电路都正常工作,是否只有这一两片样品存在此问题,其它芯片会是一样的现象吗。另外可以看各个电源的PIN脚有没有存在漏电,特别是看看decouple电容有无损坏。如果你们有当地代理商的FAE支持的话,可以叫他现场看看。
你好,有没有比bq24600更简单的,能充3串联锂电池的充电芯片。如果有,请帮忙推荐。
Thanks!
你好,能否发一份BQ24133的应用电路图给我(或你们的评估板电路图),充电电流大概2A,充3串联锂电池。
Thank you!
NathanXiang
如下的EVM板使用手册中所示的电路可以配置为12.6V 2A的充电器。