This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3488调试求助,电源上会有锯齿波

Other Parts Discussed in Thread: LM3488, LM3481, LM3478

输入输出要求:输入电压范围3.3V~6.0V,输出电源为5V,1.0A

利用TI的WEBENCH设计的一个电源,芯片是LM3488。

一些器件不好找,做了些替换

MOS管用的IRF7807,二极管用的MBRS430T3,

电感SRU1038-6R2Y  替换为SLF1045-6R8Y  ;  VLC5045T-220M 替换为 LTF5022T-220M

Rsense 0.025欧姆, 替换为0.03欧姆

焊接之后上电检测,发现电源上会有锯齿波,周期约为200ms ,幅度约为0.2V   请问该如何调整?

上传的两个附件,一个是WEBENCH自动生成的,一个是修改后的(自动生成的那个原理图太难看了)。

power.rar