This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH提供的PCB参考的问题

Other Parts Discussed in Thread: LM2677

做一个24V转12V 4A的DC-DC。

上TI的在线设计软件 WEBENCH辅助设计,利用LM2677给出的原理图和PCB见附件

 

问题1:为什么推荐的PCB板图中的引脚4 没有连接到GND。但是8连接到GND了。8就是为了散热的么。

问题2:我自己画PCB的话,要严格按照这个PCB的尺寸来么?我只把接地的那片覆铜  做大,不影响散热能行么?其他的线适当加宽,可以么?