请问,Xilinx的开发板ZC702,ucd9248控制PTD08d210W模块电压,PTD的B路没有电压输出是怎么回事?U21和U19本应输出2.5V和1.5V,但是输出的分别为0.25V和0V ,也没有发生短路,用TI USB重新烧录了程序,结果还是一样。
另外,测试了UCD的3.3V是正常的,如果PTD损坏,根据哪个引脚可以判断?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问,Xilinx的开发板ZC702,ucd9248控制PTD08d210W模块电压,PTD的B路没有电压输出是怎么回事?U21和U19本应输出2.5V和1.5V,但是输出的分别为0.25V和0V ,也没有发生短路,用TI USB重新烧录了程序,结果还是一样。
另外,测试了UCD的3.3V是正常的,如果PTD损坏,根据哪个引脚可以判断?
Manufacturing Tool调试问题时不如下面这个软件灵活,可以下载安装调试。使用该软件可以在monitor菜单中看到单板的故障,即为何没有输出。