看到TPS79901数据手册里描写的压差如下:
其中Vin=Vout(NOM)-0.1V这一项怎么理解呢?Vin比Vout(NOM)低么?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jerry Tang 说:各位,
有没有相关的测试方法可以参考一下,这样更加清楚一些。
谢谢!
提供一种方法供参考,通过分压电阻将Vout设置到3.3V,先将VIN升至4V,此时输出电压为3.3V,输出电流设置成100mA。
将VIN降至3.2V,Vout也会随之下降,VIN-Vout的值也就是这个电压。