This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9222+UCD7242电压无法出1V

Other Parts Discussed in Thread: TMS320C6678, UCD9222, UCD7242

各位专家好:

      我仿照EVM板通过UCD9222+UCD7242的形式给两片TMS320C6678提供AVS,进入fusion digital power designer,以后都显示正常,但是在USB control选项置高以后,Vout却始终拉不上去,同时会有TON_MAX fault,Iout会飙升到9A,duty circle达到98%。请问这可能是什么问题引起的?

注:同样的软件设计在另一块板上验证过了,焊接也是相同的。

  • 你好,Iout的值和duty circlye的值都是在GUI的Monitor菜单中读到的是吧?

    如果能确认软件设计没有问题,可以重点排查下反馈电阻(EAP/EAN引脚处)是否虚焊。输出电感有无虚焊。

    在调试时,可以将限流点(fast OC fault / OC fault)设置的低一些,防止烧机。