Other Parts Discussed in Thread: GPCRB
在最后从9%,快速降低到0%,中间5%的电量跳过了,具体数据请看附件LOGO数据。new-低温15W-2-×.log
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,是否用GPCRB做过低温补偿
When you use the GPCRB tool it is optimizing for the data provided, with this kind of low temperature any small changes can impact accuracy greatly, it is tuned for that specific pack to get the highest accuracy, when it is used with other packs at this low of a temperature I would expect the variation in cells to lead to a couple percent error