This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61085有两种大小不同的封装MSOP和TSSOP,参数不一样吗

Other Parts Discussed in Thread: TPS61085

在我的应用里需要将锂电升压到12V驱动3.5W的电磁阀。

在TPS61085数据手册里有3.3升压到12V输出600ma的应用。

但我发现TPS61085有两种大小不一样的封装MSOP-8和TSSOP-8,两者在经销商那边的报价也是有点差别的。

我就想知道这两种封装在性能上有什么区别,都可以在3.3升压到12V输出600ma电路上应用吗。

MSOP-8这个封装会不会散热上有点不足呢。

  • 1. TPS61085两种封装在参数上一样,不同在于封装不同,热阻会存在差异,但是这个差异并不大:MSOP  181°C/W  -----TSSOP 160°C/W,   封装差异应是价格偏差的原因。

    2. 按照datasheet:  www.ti.com.cn/.../tps61085.pdf 第五页Figure 1. 3.3V转12V/电流是达不到600mA.  按照13页的应用图算出来MOS的最大电流都在3A左右,而按照参数:ILIM 是2.0~3.2A, 显然这里是按照最理想可能出现的最大电流,而按照实际应用设计,MOS的电流不应该超过2A.  所以如果是600mA输出,两者都会出现问题。

    3.  按照您的应用, 3.5w输出,效率85%,损耗是618mW, 这个功耗已经很大了,按照datasheet第二页的DISSIPATION RATINGS,只适用于常温TSSOP封装。

    4.建议频率设计650kHz,TSSOP封装芯片。可以实现较高频率,芯片发热也会小一点。

  • 你好:

       不同的封装的散热效果不一样。可以查看手册中的第2页。封装不同,但仍足以解决散热问题,只要PCB布板时,加些0.3毫米-0.33毫米的过孔。可参考附件中的布线指南。

    www.ti.com/.../tps61085.pdf

     

    NS经典的DCDC_PCB_布局指南.pdf