This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24600

Other Parts Discussed in Thread: BQ24600

    小弟在制作锂电池充电器过程中遇到一点问题,请各位大虾帮忙处理下!AC/DC模块,小弟想选用输出9V、1100mA的小功率模块,但是对于给BQ24600供电的电流不知道该选用多大合适,小弟锂电池电压是4.3V、1.5A,原理图我贴上,求各位大虾帮忙看下有无设计问题。。。还有中间SIR426DN这个N-Channel-MOSFET,可以用什么样的晶体管进行替换。如果可以,给小弟留个QQ或者其他联系方式。。。多谢!

充电器原理.SCH
  • 你好,关于AC-DC的模块,由于power path所以只要满足大于1.2*Ioutmax就可以了,这样也可以避免充电器前端需要比较大的输入电容,这里的Ioutmax就是ICC。谢谢!

     

  • 电池这一块,请您看一下规格书,看看你的电池的容量是多少,然后看看其建议的最大充电比率是多少C,一般是0.5C,但目前已经有支持大比率充电的电池。

    确定了ICC 以后就代入到上面的Ioutmax ,谢谢!