按照TI设计软件搭的TPS40210 boost电路,从24V升到200V,输出电流设计为0.2A。一直以为电路出现问题,结果是芯片的问题。。。费了很大劲
现在可以达到24V到190V左右了。不过新的问题又来了:
空载电压190V,带上负载电路后电压一直将到零!而且断了电源也不恢复。
我的负载电路是一个考毕兹振荡电路,很想知道问题出现在哪里?是电流不够么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢你的回答。
我一直很想知道我所搭建的boost电路是工作在什么模式下。按照TI公司“Understanding Boost Power Stages...”这篇文章里讲的Lmin>VoTs/16*Io(crit)(不知道Io(crit)是不是指Vo/R,R是最后的分压电阻?),那么该boost 电路工作在DCM模式下。。。
如果要想工作在CCM模式下,我得将电感增大到10.7mH。。。不知道这么推对不对
该电路输入电容是10uF/50V,应该不大吧,事实上电源带载能力不行。。。问题还可能出现在哪里呢?设计的是0.2A输出电流应该够用的了
之前用另一款boost芯片搭的电路没出现过这种问题,当时测的输入电压也是24V,输入电流1A多一点。输出都上300V了。(TPS40210最大260V啊)