Other Parts Discussed in Thread: LM2841, ADS1148, LM25018, SM72442
这个电源芯片是给ADS1148供电,要求输入24V直流,输出双电源±2.5V ;因为要采集正负电压,所以供电有点麻烦,最好有双通道的芯片,没有的话两片分开也行,求TI支持!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
推荐使用LM2841,SOT封装,外围也非常简单。
+2.5V电路可参考TI在线仿真软件Webench设计:http://webench.ti.com/webench5/power/webench5.cgi?VinMin=26&VinMax=26&O1V=2.5&O1I=0.20&base_pn=LMR14203X&AppType=None&op_TA=30&lang_chosen=en_US&optfactor=3
-2.5V设计只需将以上设计稍作改动即可,见下图。
楼主您好!
根据您的描述,±2.5V的电源是给ADS1148的模拟部分供电的,电流在1~2mA。由于是对AD供电且是正负电源,所以供电方案我建议是 从24V用开关电源产生 ±5V, 再由±5V通过LDO产生±2.5V。
具体方案是:
1. 用LM25018 从24V产生两路电源:±5V;
2. 用LDO :TPS79225、TPS72325从±5V得到±2.5V电源(详情可参考http://www.ti.com.cn/cn/lit/ug/sbau142b/sbau142b.pdf)
希望对您有帮助!