This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

开关DC/DC咨询

Other Parts Discussed in Thread: TPS61030

请问ti工程师,我查到ti的开关DC/DC芯片,TPS61030PWPR,它可以稳定提供3.6A的电流输出么?还是提供一个瞬时的电流?我想用这个片子给我GPRS模块供电,要求dc/dc提供至少3A的电流。我设备的尺寸有限制,想用一节锂电池,或者两节干电池串联。这个芯片可以在输入电压降低到1.8V还能够给出稳定的电压和电流输出么?

  • 最低1.8V输入,输出是几V?5V吗?如果输出是5V 3.6A,按90%的转换效率(实际上达不到)来计算,那输入为1.8V时输入电流将达到11A,没有哪个干电池能达到这个放电电流吧;你的GPRS模块应该没有需要这么大电流的,你再查清楚看看。--非TI工程师(捷恩斯威科技(www.jeansway.cn)AE--彭博)

  • TPS61030它的开关峰值限流是4A(min=3.6A),考虑电感上的纹波电流,它是不能够提供3.6A电流输出的。

    TPS61030可以在1.8V的情况下工作,但对于boost电路,如果先不考虑效率Iin=(1-D)*Iout,输入电流等于电感电流等于开关管电流,所以当输入输出电压差较大的情况下,能提供的负载电流是肯定小于3A的。

  • 同意二楼的回复。

    按照我的理解,GPRS模块工作应该是TDM,估计每八个周期工作一至二个。如果是这样的话,平均输入输出电流应该没有这么大。

  • 3A的电流已经很大了,二楼的解答很正确,你再确认下你的系统对电流的要求.tps61030在1.8V是输出的最大电流在1A左右。

x 出现错误。请重试或与管理员联系。