请问ti工程师,我查到ti的开关DC/DC芯片,TPS61030PWPR,它可以稳定提供3.6A的电流输出么?还是提供一个瞬时的电流?我想用这个片子给我GPRS模块供电,要求dc/dc提供至少3A的电流。我设备的尺寸有限制,想用一节锂电池,或者两节干电池串联。这个芯片可以在输入电压降低到1.8V还能够给出稳定的电压和电流输出么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最低1.8V输入,输出是几V?5V吗?如果输出是5V 3.6A,按90%的转换效率(实际上达不到)来计算,那输入为1.8V时输入电流将达到11A,没有哪个干电池能达到这个放电电流吧;你的GPRS模块应该没有需要这么大电流的,你再查清楚看看。--非TI工程师(捷恩斯威科技(www.jeansway.cn)AE--彭博)
3A的电流已经很大了,二楼的解答很正确,你再确认下你的系统对电流的要求.tps61030在1.8V是输出的最大电流在1A左右。