This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54561 PWRGD问题



芯片电路目标输出5V 3A,参考手册的使用电路,VIN=24V,Vout=5V,配置阻容和参考电路是一致,除了EN引脚的90K左右的换成53.6K,PWRGD引脚是24V 串接1k电阻  +串接LED,经测量EN引脚电压是2.4V左右,输出是5.04V,问题是PWRGD导通了,就是串接的LED变亮了,这显然是个异常状态,电路是没有过压的,输出后级电路让我断开了,也就是空载,用直流稳压源,实时功率是24V,0.06A,也没有过流,芯片也没发热,所以奇怪的是为什么PWRGD会导通到地?   请帮忙分析下