This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210 不工作

Other Parts Discussed in Thread: TPS40210, UCC27324

偿试把第三脚直接接到地,R23,短路,结果都一样,输入电压为11。8V,不带负载,电压会从12V左右慢慢升到输出电压为20V,左右,只要一带负载,哪怕是很小的负载,输出电压变成11。3V左右,好象是输入与输出之间直接通过二极管输出一样。GDRV,用万用表量测为0V,BP,脚为8.1V;SS脚为电压在1V内变化。PCB是两层板,我看EVM是4层。一直不知道是哪里原因,感觉IC没有工作一样。

请大虾多指教。