This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教BQ27510的无ev2300下校准过程



我查看了slua415,关于Impedance Track校准过程。在文档中,有几个地方不明白,请教:

1、文档中的校准使用的是i2c命令中的子命令,文档中第一步效验是电压和温度同时进行。请问是否可单独效验电压或温度?

2、文档中使用的例子是校验外部温度传感器的。如果校验内部温度传感器,是否校验值还是放在0x0c、0x0d这个2个子寄存器?

3、请问这些寄存器是否有清单?如果有,请问是在哪个文档中?

4、中间有一个步骤是判断是否校验完成,使用的命令是:”Read Address 0x02 Is value 0xC000“,这个步骤的I2C命令序列是否是:start,0xaa,0x00,0x02,0x00,stop;start,0xaa,0x00,restart,0xab,(read),(read),end?

5、新G3版的BQ27510貌似比G2版多出了很多参数选择,请问文档SLUUA97”bq27510-G3 Technical Reference Manual”哪里可以下载?

6、G3版中基本寄存器从bqView中查看,多处了好几个"true"的寄存器,请问这些寄存器和原来的有什么区别?

谢谢您的回复!