This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430

Other Parts Discussed in Thread: TPS5430

TPS5430,当输入电压为6V时,不能正常输出为4.8V,1A时.

按官方设计软件,却是完全可以达到的.原理图和PCB布局都是按照设计软件自计的设计.

TPS5430,之前从9V-30V稳5V   或者说从30V稳12V都是没有问题的.该器件已经使用了20K了.