This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1: HDQ Pin in INTERRUPT Mode

Part Number: BQ27542-G1
Other Parts Discussed in Thread: BQSTUDIO

Hi TI expert,

We turn off the Battery Trip Point Interrupt Function by setting BTE_EN to 1.
When the RC has crossed below the set threshold,The Flags()[SOC1] bit is set to 1,but the interrupt didn't asserts on the HDQ pin.
Then we tried to Set the [HOST_IE] bit to 1 and issue SET_HDQINTEN through BqStudio, but it didn't work.
Attached is the GG file,please help check,thank you!

 5859104-1.gg.csv