我们使用了TPS2121用于2路12V输入的切换。以下为我们设计的原理图

当IN2的电压输入为10V,IN1输入从10.5V上升到12V的时候,输出12V会出现跌落的现象,导致板子重启。
测试的情况负载电流比较大,在3A左右。

输入IN1和IN2使用的都是直流稳压电源,输入端电压用示波器测量过都没有跌落。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
如果用电源供应器直接切换到12V, 而不是缓慢上升到12V,上述现象是否依旧?
另外你可以看一下datasheet 第15页9.3.7.
我们现在测试都是IN1的电源12V直接降到10.5V,和10.5V直接升到12V的。不是缓慢上升和下降。
如果IN1直接从12V降到0,或者从0升到12V是没有这个问题的。datasheet第15页9.3.7里面说明下降的时间只有5us的下降, 不像我们测试有30ms的下降。
另外这ST信号昨天测试还切换的时候是能从3.3V跳到0V的,今天发现切换的时候ST信号只是拉低了一点,并没有输出0V。
换了一个TPS2121芯片,ST信号变成了10V多了,电压跟着IN1变化了。感觉ST电平不稳定
HI
参考评估板,将输入电容放小一些,尽量靠近芯片IN脚。
HI
对照评估板电路改一下输入看看,其他电路看起来没有什么问题,因为电路配置本身很简单。输入很容很大,会导致输入电压变化速度较慢,而输入电压侦测本身对输入源选择有影响。
HI
The ST pin can be pulled high with a resistor to provide feedback on the status of the system. If the status pin is high, IN1 is the output. If the pin is low, IN2 is the output. If this feature is not required, the ST pin can be connected to GND.
所以如你所说,ST信号切换到IN2的时候,芯片内部是拉到地的。