This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: TPS2121 输出跌落的问题

Part Number: TPS2121


我们使用了TPS2121用于2路12V输入的切换。以下为我们设计的原理图

当IN2的电压输入为10V,IN1输入从10.5V上升到12V的时候,输出12V会出现跌落的现象,导致板子重启。

测试的情况负载电流比较大,在3A左右。

输入IN1和IN2使用的都是直流稳压电源,输入端电压用示波器测量过都没有跌落。