This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z100 flash 配置的参数选择

Other Parts Discussed in Thread: BQ34Z100

电池组是16节磷酸铁锂串联,每节电池电量100Ah,电压3.3V,

现在利用EV2300配置bq34z100 FLASH DATA ,

配置design capacity =500mAh

design energy=26400 design energy scale=1 

qmax cell0=500mAh

这样 相当于系数是200

其他是电压的配置。

这样,我在校准电流时,如果放电实际电流是20A,那么我校准值就是-100mA。但是校准时总提示 run-time error over flow!

我的疑问是:

 1 在flash 配置时,是否还需要配置其他电流 电量相关的信息。例如 sleep current,taper current等。如需配置,是否应按这个200系数来配置。

2 如果我把design energyscale 设10 ,应该配置哪些东西?

3 这里design cap =500mAh,是不是太小了?

谢谢