This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24170调试失败

Other Parts Discussed in Thread: BQ24170

参照BQ24170 DATASHEET 电路,制作3节锂离子电池充电电路,装配后测试,出现以下现象,插入适配器(13.5V)后,LED闪烁,SYSTEM端能测出输出电压,带上负载后

输出电压变成1V左右,发下是ACFET关闭。去掉适配器使用电池带负载,工作正常。测试芯片VREF输出为3.6V,与手册3.3V差别过大。充电功能就更不用提了。想问下,这是怎么回事?目测电路外观正常,无短路、虚焊现象。

  • 你好,

    bq24170datasheet 中给出了4种应用电路,不知您是按哪种设计的,能否提供电路图?

    在插入适配器而不接电池时,bq24170会检测的battery absent,LED闪烁。若是按Figure3的应用电路,System这是的电压波形应该与Figure21类似,内部恒流源对battery端的电容充放电。当加载后,就会将battery和system的电压拉低。

  • 我是参照第一个典型应用设计的,我的问题是1、参考电压Vref为什么误差那么大,3.6V;2、使用适配器接上负载后,ACFET关闭,输出电压降低,使用电池带负载正常。稍后我把原理图贴上,谢谢!

  • 你好,

    从电路图看,在VREF和REGN处都选用1uF电容都是没有问题的。不知REGN的电压是否是正常值?如果更换芯片也是同样的问题,那有可能是layout的问题,附件是bq24170EVM的user's guide,里面有layout guideline和实际layout的示意图,可以和您的layout对比。AVCC,VREF,REGN去耦电容的引线要尽可能的短。

    bq24170EVM.pdf
  • 谢谢您的回复!REGN不正常,为6.6V。BQ24170的EVM我也看了,布线时就是参考了它的布局。当时有就有一个问题很迷糊。

    在DATASHEET中
    关于功率地和模拟地的连接的论述:
          Route analog ground separately from power ground and use a single ground connection to tie charger power
    ground to charger analog ground. Just beneath the IC use analog ground copper pour but avoid power pins
    to reduce inductive and capacitive noise coupling. Use the thermal pad as a single ground connection point
    to connect analog ground and power ground together, or use a 0-Ω resistor to tie analog ground to power
    ground. A star-connection under the thermal pad is highly recommended.功率地和模拟地通过散热焊盘连接,或者通过
    0欧姆电阻连接。
         在EVM中,有这样的论述:
         The control stage and the power stage must be routed separately. At each layer, the signal ground and
    the power ground are connected only at the thermal pad. 功率地和模拟地仅在散热焊盘连接。
    我的是在中间层(功率地)分割出一块模拟地,这块地和散热焊盘连接,然后通过0欧姆将此分割地和
    功率地连接。如下图所示:
         这种布局或不会影响到Vref的输出?盼望回复!
  • 问题解决了,如果THERMAL PAD 没有焊的话,就会出现这种现象!

  • Good news.

    您之前贴的图看不到了,方便的话可以重新贴一个,做一个分享。谢谢。