参照BQ24170 DATASHEET 电路,制作3节锂离子电池充电电路,装配后测试,出现以下现象,插入适配器(13.5V)后,LED闪烁,SYSTEM端能测出输出电压,带上负载后
输出电压变成1V左右,发下是ACFET关闭。去掉适配器使用电池带负载,工作正常。测试芯片VREF输出为3.6V,与手册3.3V差别过大。充电功能就更不用提了。想问下,这是怎么回事?目测电路外观正常,无短路、虚焊现象。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参照BQ24170 DATASHEET 电路,制作3节锂离子电池充电电路,装配后测试,出现以下现象,插入适配器(13.5V)后,LED闪烁,SYSTEM端能测出输出电压,带上负载后
输出电压变成1V左右,发下是ACFET关闭。去掉适配器使用电池带负载,工作正常。测试芯片VREF输出为3.6V,与手册3.3V差别过大。充电功能就更不用提了。想问下,这是怎么回事?目测电路外观正常,无短路、虚焊现象。
你好,
从电路图看,在VREF和REGN处都选用1uF电容都是没有问题的。不知REGN的电压是否是正常值?如果更换芯片也是同样的问题,那有可能是layout的问题,附件是bq24170EVM的user's guide,里面有layout guideline和实际layout的示意图,可以和您的layout对比。AVCC,VREF,REGN去耦电容的引线要尽可能的短。
谢谢您的回复!REGN不正常,为6.6V。BQ24170的EVM我也看了,布线时就是参考了它的布局。当时有就有一个问题很迷糊。
问题解决了,如果THERMAL PAD 没有焊的话,就会出现这种现象!
Good news.
您之前贴的图看不到了,方便的话可以重新贴一个,做一个分享。谢谢。