This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm3489 使用相关问题

Other Parts Discussed in Thread: LM3489

想用lm3489 设计一款可调电源 要求Vin:4.5~25V,Vout=4.5~20V,Iout最大能到4A,从选型列表参数中看起来这款controller是可以符合要求的

目前有如下疑问:

1、Vout=Vin,且Iout=4A时,能够正常稳定工作吗

2、由于PMOS是外置的,那可不可以理解为Iout最大电流主要取决于PMOS能过多大电流(当然还有电感等...),

那如下图选型列表中为什么会标注Iout MAX=4A,是不是IC内部有其他什么因素限制了MAX电流?