Part Number: LMR64010
设计要求:
输入电压:4.5V-5.5V
输出电压:7V
输出电流:Imax=50mA
使用10uH电感时,电感电流出现负值,不知道为什么?实际这样使用是否有问题?

使用20uH电感时,电感电流正常

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
电感计算直接参考datasheet即可(datasheet第10页),电流按照满载50mA计算。
或者你按照芯片官网的在线仿真webench来设计电路。