This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR64010: 示波器测试电感电流出现负值

Part Number: LMR64010


设计要求:

输入电压:4.5V-5.5V

输出电压:7V

输出电流:Imax=50mA

使用10uH电感时,电感电流出现负值,不知道为什么?实际这样使用是否有问题?

使用20uH电感时,电感电流正常