This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8764-Q1: LP876411B4RQKRQ1 jitter issue

Part Number: LP8764-Q1


Hi TI team,

Each rail’s jitter waveform as attached, we found it is failed (over 15%) on the PMIC solution (LP876411B4RQKRQ1).

Do you have advice to improve the result?

Order number: LP876411B4RQKRQ1

Input voltage: 5V

Output voltage: 1.1V

Iout: 0A & 3.2A

Fsw: 2.2MHz

Lout: 1uH

Thank you.