Hi TI team,
Each rail’s jitter waveform as attached, we found it is failed (over 15%) on the PMIC solution (LP876411B4RQKRQ1).
Do you have advice to improve the result?
Order number: LP876411B4RQKRQ1
Input voltage: 5V
Output voltage: 1.1V
Iout: 0A & 3.2A
Fsw: 2.2MHz
Lout: 1uH

Thank you.