Part Number: BQ40Z80
Other Parts Discussed in Thread: BQSTUDIO
学习成功过的bq40z80,LStatus状态位为06;充满电后(FC置1,SOC=100%)静置6天,期间不充电不放电不通讯,bq40z80处于sleep模式;
为什么6天后再次通讯SOC会在静置阶段下降至93%?该怎么避免这种情况的发生?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
QH-BMS-9686-6S-V1.0-2023-3-22.gg.csvroomtemp_rel_dis_rel-report.zip化学ID用的是2087,最新版的上位机与ID库没有5930
您好,BQSTUDIO的下载页面可以下载最新的Chemistry update。
温度下降超过5度会重新计算容量等参数,建议您放温箱验证一下是不是这个问题造成的。
您好,请参考下面内容
Over the 6 days is there any self discharge or loads on the battery? From the chem ID report it looks like it was a good match so the relaxed voltage should correlate with less than 2% max error. Can they share a short log of before and after so we can see all the registers from the test? What makes them think that the RSOC is not actually 93% due to self discharge/system load?
您好,CC DeadBand is a threshold which decides if the output from the CC is added to the total passed charge. The main purpose is to extract useful data from the CC for very small measurements which are close to the noise floor of the CC.
CC deadband 如何计算正在查询,稍后回复。