在2欧姆负载上,
(1)输出电压不超过5V,不低于1V;
(2)在输出电压为5V时,尽可能减小输出电压纹波;
(3)在输出电压为5V时,DC-DC电源效率应大于85%;并尽可能提高效率;
加入单片机控制。在2欧姆负载上,实现输出电压灵活可调,
(1) 通过按键改变输出电压,以1V为步进,从5V输出,降低为1V输出;
(2) 在1V输出电压下,尽可能提高DC-DC电源的效率;
(3) 更换负载电阻为500欧,调节输出电压为5V,尽可能提高电源的效率;
可以给我一个思路吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
用INA209可以检测你输出的电压和电流值,这些值可以通过MCU判断出负载情况。
(1) 通过���键改变输出电压,以1V为步进,从5V输出,降低为1V输出;
改变电压的方法是,MCU根据按键和INA209检测到输出的情况控制一个DAC101的输出,这个输出通过一个电阻接到开关电源的FB点。输出电压和DAC的电压关系满足这一点的电流恒定定理。
(2) 在1V输出电压下,尽可能提高DC-DC电源的效率;
MCU根据INA209检测到输出电压为1V时,输出一个较低的频率同步开关电源的开关频率,这样频率降低了,效率就高了。
(3) 更换负载电阻为500欧,调节输出电压为5V,尽可能提高电源的效率;
MCU根据INA209检测到的电压电流值计算出负载大小,如果为500ohm,则通过DAC调整输出为5V。
开关电源芯片推荐参考电平低得可以同步的tps54620或者LM25117这种。
用INA209可以检测你输出的电压和电流值,这些值可以通过MCU判断出负载情况。
(1) 通过改变输出电压,以1V为步进,从5V输出,降低为1V输出;
改变电压的方法是,MCU根据按键和INA209检测到输出的情况控制一个DAC101的输出,这个输出通过一个电阻接到开关电源的FB点。输出电压和DAC的电压关系满足这一点的电流恒定定理。
(2) 在1V输出电压下,尽可能提高DC-DC电源的效率;
MCU根据INA209检测到输出电压为1V时,输出一个较低的频率同步开关电源的开关频率,这样频率降低了,效率就高了。
(3) 更换负载电阻为500欧,调节输出电压为5V,尽可能提高电源的效率;
MCU根据INA209检测到的电压电流值计算出负载大小,如果为500ohm,则通过DAC调整输出为5V。