1.不论是看datasheet还是一些文章,L1和L2都是相等的,为什么webench上面计算的两个电感值是不同的?具体该如何计算?
2.Rramp的作用是什么?作用到底有多大?没有是否可以?
3.Cs具体是如何选取的?大部分只说了有效电流,然后就出了一个值,为什么?
4.补偿是如何计算的?
请大神帮忙解答!非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
speic中一般用耦合电感的方式来提高效率,所以一般都建议2个电感大小相等。如果用分立的2个电感的话,数值是可以不同的。data sheet第22页也有说明 "If L1 and L2 are wound on the same core, then L1 = L2 = L. All the equations above will hold true if the inductance is replaced by 2L.”
计算方法的话可以参考data sheet 公式43和44。
Cs的话是用来保证L1和Cs的能量平衡的. Cs在MOS管导通阶段泄放的能量等于L1在MOS关断时间内给Cs充电的能量.而Cs的电压变化和L1的纹波电流的计算就可以参考公式51和52,就可以计算出Cs的值了
你好,请注意此处CS上的纹波电流比较大,选取CS时需要选esr小的耐流够的电容,CS的计算你可以由Ic=Cducs/dt得到,谢谢。