This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478 speic (3~24-->5)的一些疑问(为什么通过邮箱点击链接显示被删除?)

Other Parts Discussed in Thread: LM3478

1.不论是看datasheet还是一些文章,L1和L2都是相等的,为什么webench上面计算的两个电感值是不同的?具体该如何计算?

2.Rramp的作用是什么?作用到底有多大?没有是否可以?

3.Cs具体是如何选取的?大部分只说了有效电流,然后就出了一个值,为什么?

4.补偿是如何计算的?

请大神帮忙解答!非常感谢!

  • lm3478刚好最近用过。 第一个问题,lm3478有两种典型应用模式,dcdc电源有六种拓扑结构。 手册上应用两个电路的采用sepic和boost。ti.的仿真软件,采用boost就是芯片手册第一种。 第二个问题和第三个问题,没有看到电路图。-_-||.如果是指接在comp pin的电阻的话,那是指调节稳定性的,在其他芯片手册上见到过,一般这个引脚接的电阻和电容都是有典型值的,一般都是越小稳定性越好。 第四个问题,我没有看懂,说的是回路补偿电路吗?电流模式的电源芯片在占空比大于0.50时转换器会在开关频率的次谐波频率点震荡(没有使用斜坡补偿电路)。这个好像不用担心。 以上是对该芯片的一点点理解希望可以帮到你,如果有什么不正确和不足的地方,请指正。共同学习。
  • speic中一般用耦合电感的方式来提高效率,所以一般都建议2个电感大小相等。如果用分立的2个电感的话,数值是可以不同的。data sheet第22页也有说明 "If L1 and L2 are wound on the same core, then L1 = L2 = L. All the equations above will hold true if the inductance is replaced by 2L.”

    计算方法的话可以参考data sheet 公式43和44。

  • Cs的话是用来保证L1和Cs的能量平衡的. Cs在MOS管导通阶段泄放的能量等于L1在MOS关断时间内给Cs充电的能量.而Cs的电压变化和L1的纹波电流的计算就可以参考公式51和52,就可以计算出Cs的值了

  • 你好,请注意此处CS上的纹波电流比较大,选取CS时需要选esr小的耐流够的电容,CS的计算你可以由Ic=Cducs/dt得到,谢谢。