This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596: 关于LM2596设计的问题

Part Number: LM2596


需要设计一个正负可调的电源,输入直流36V,输出为正负30V左右可调,

目前的问题为能否将两个LM2596芯片输出串联共地的方式达到设计目的,输出三端分别为正负和地,

二者输出串联的话,两个芯片可以输入可以连一起吗,或者有什么别的芯片可以推荐